Starting with version 0.12.6 for ROS1 and version 0.12.7 for the ROS2 branch the ouster-ros driver supports automatic sensor re-connection, which allows users to:
- start up the driver before booting up the sensor
- recover connection to the sensor after connection was dropped (wire disconnected)
- recover connection to the sensor after sensor power cycle
In case this case the driver will reset configuration to persisted config
To enable this feature set the attempt_reconnect ros launch parameter to true (disabled by default). To have control some control over the frequency of attempts users can make uses of the two additional params:
dormant_period_between_reconnects: time to wait between reconnect attempts, default is 1.0 secondmax_failed_reconnect_attempts: maximum reconnect attempts, default is 2147483647
Here few of demos of how this feature works
- auto reconnect after wire was disconnected
- change config via
/ouster/set_configservice call, then power cycle the sensor
- change the sensor configuration via the sensor config page