Correcting slow rotational drift in multi-mile Ouster SLAM runs without smearing geometry

We are processing multi-mile, vehicle-mounted OS1-071-64U-ASR Rev7 data using firmware 3.2.0, SDK 1.0.1, ACCEL32_GYRO32_NMEA, PPS synchronization, and a PPS-aligned PolyNav dual-antenna GNSS/INS.

The Ouster SLAM cloud is often internally very clean: pavement, poles, wires, and vegetation remain sharp. However, over a multi-mile run, the cloud can gradually turn or float right/left relative to the road and GNSS/INS trajectory. The apparent attitude difference is commonly about 1-6 degrees, occasionally more.

We divide long runs into approximately 500-ft local pieces. Within those bounded pieces, sparse external position authority can improve placement without visibly deforming the cloud. The 500-ft length is an operational bound that has worked for position correction; it is not yet a validated rotational-correction length.

What we have tried

1. One rigid transform for the full run

We solve one constant transform between the Ouster SLAM world and the external projected frame:

Texternal=Talignment⋅TSLAMT_{external} = T_{alignment} \cdot T_{SLAM}

Every pose receives the same rigid transform. This preserves the cloud’s internal geometry, but it cannot correct attitude drift that changes over a multi-mile run.

2. Dense external-attitude correction

We transformed both the PolyNav attitude and the Ouster body_to_world attitude into a common external world frame and the same Ouster sensor-body frame, including the fixed vehicle-body-to-Ouster-sensor extrinsic rotation.

Conceptually, for each LiDAR pose at time tt, we formed a time-varying rotational delta:

ΔR(t)=Rexternal,sensor(t)⋅Raligned_SLAM,sensor(t)−1\Delta R(t) = R_{external,sensor}(t) \cdot R_{aligned\_SLAM,sensor}(t)^{-1}

Here, aligned_SLAM means the Ouster SLAM attitude after applying the single rigid SLAM-world-to-external-world alignment.

We then applied that delta to the aligned SLAM pose:

Rcorrected(t)=ΔR(t)⋅Raligned_SLAM,sensor(t)R_{corrected}(t) = \Delta R(t) \cdot R_{aligned\_SLAM,sensor}(t)

Conceptually, this makes each LiDAR pose follow the external GNSS/INS attitude.

It improves apparent road alignment, but it smears poles, wires, pavement, and other fixed objects. The time-varying rotational correction changes inside sections that were originally internally consistent, so it twists the geometry rather than moving it rigidly.

3. Local bounded position optimization

We use approximately 500-ft pieces with sparse external position controls. This has improved placement while retaining sharp local geometry. We deliberately avoid dense per-column translation, vertical warping, and dense attitude replacement.

What we need to solve

We do not need every LiDAR pose to exactly equal the GNSS/INS attitude. We need to correct slow accumulated rotational drift across the multi-mile run while retaining the rigid internal geometry of each clean local section.

Our questions are:

  1. Is the appropriate model to solve one rigid SE(3) correction—rotation plus associated translation—for each approximately 500-ft piece, then solve a sparse, continuous chain of those corrections across the full multi-mile run?
  2. Can PoseOptimizer accept sparse, low-weight external attitude controls at selected stable locations or piece boundaries, rather than at every LiDAR pose, without twisting geometry inside each piece?
  3. What is the recommended procedure for establishing the common frame between:
    • PolyNav body/INS attitude,
    • vehicle body frame,
    • fixed Ouster sensor extrinsics,
    • and Ouster SLAM world frame?
  4. Is there a preferred Ouster approach for deriving and applying one rigid rotation correction per piece from body_to_world poses and external INS attitude?
  5. What validation would you recommend before accepting a correction? Our acceptance criteria would be improved road and pole alignment while confirming that wire sharpness, pole verticality, pavement geometry, and piece-to-piece seams do not degrade.

Our requirement is that every local correction remain rigid within its validated piece, with translation and rotation solved together so seams remain continuous. We need to avoid per-column or dense per-pose attitude replacement that warps an otherwise clean cloud.

I would recommend to use PoseOptimizer. Add your PolyNav solution as sparse, low weight absolute position constraints through the Python API, then add loop closures if the route
revisits the same area.

Below is add absolute position constraints (GPS) example. You dont want to add constraint to every lidarframe. SLAM has much better accuracy for short distance. Try with parameter min_distance_m meanwhile keep the GPS constraints very low weight so the local geometry stay sharp

for ts, xyz in gnss:
pose = np.eye(4)
pose[:3, 3] = xyz
po.add_constraint(mapping.AbsolutePoseConstraint(
timestamp=np.uint64(ts),
pose=pose,
rotation_weight=0.0,                               # position only, no attitude
translation_weight=np.array([0.01, 0.01, 0.001])))  # low weight, softer on Z

po.initialize_trajectory_alignment()  # one rigid SLAM-world -> GNSS-frame alignment
po.solve()

po.add_relative_loop_constraints(min_distance_m=50.0, cell_size_m=2.0, icp_score_threshold=0.6)
po.solve()

po.save("optimized.osf")

You can visually check the relative_loop_constraints by ouster-cli command
ouster-cli source slam_output.osf pose_optimize --auto-loop optimized.osf
Make sure there is no wrong loop pairs added