Time synchronization using PPS and NMEA over ethernet

Hi,
I’m looking into the possibilities to replace a VLP16 by a OS1.
For this I would like to synchronize the time of the OS1 using a PPS and an ethernet NMEA GPRMC message. Is that possible? (with the VLP16 it was)
Regards Walter

1 Like

The OS1 accepts the same time synchronization inputs as the VLP16. Please review the following section of the Firmware Users Manual:

Thanks for you response, I had a look at the Firmware Users Manual but couldn’t find how to configure (a port on) the OS1 to receive NMEA ethernet messages. can you instruct me?

Edit: Mean while I contacted technical support and it appears not to be possible for the OS1 to receive GPRMC NMEA messages over ethernet and use them with the PPS pulse to synchronize the internal clock !?