Data can be saved directly as CSV files in the command line interface (CLI) with the command:
-
ouster-cli source os-xx slice 0:101 save test10.csv- where
xxis the serial # of the sensor and ‘test10.csv’ is the name of the output file. - This command will save the first 102 frames as CSV files.
- where
Data can be converted from pcap to CSV formats in the command line interface (CLI) with the command:
-
ouster-cli source test11.pcap slice 0:100 save test12.csv- where
test11.pcapis the name of the pcap file andtest12.csvis the name of the output CSV file. - 101 frames (or slices) will be saved with this command
- where
Below is the key to the CSV file:
- TIMESTAMP (ns)|Timestamp in nano seconds
- ROW|Laser Channel number, Image Pixel row (0 to 127)
- DESTAGGERED IMAGE COLUMN|Image Pixel column (0 to 1023)
- MEASUREMENT_ID|Based on encoder position (0 to 1023)
- RANGE (mm)|Range for 1st return
- RANGE2 (mm)|Range for 2nd return
- REFLECTIVITY (%)|Reflectivity for 1st return
- REFLECTIVITY2 (%)|Reflectivity for 2nd return
- NEAR_IR (photons)|Photons from ambient light (not lasers)
- FLAGS|Blooming flag for 1st return
- FLAGS2|Blooming flag for 2nd return
- X1 (m)|Calculated Cartesian X coordinate of return
- Y1 (m)|Calculated Cartesian Y coordinate of return
- Z1 (m)|Calculated Cartesian Z coordinate of return