# Increase receive buffer to eliminate packet drop problem on some Windows computers

**URL:** <https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84>\
**Category:** Software\
**Tags:** ouster-studio, sdk, windows\
**Created:** [April 26, 2024, 6:00am UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84 "2024-04-26T06:00:16Z")\
**Posts on this page:** 9\
**Page:** 1

<div class="post-metadata">

**Author:** ![chris\_chen](https://avatars.discourse-cdn.com/v4/letter/c/85e7bf/32.png) [@chris\_chen](https://community.ouster.com/u/chris_chen)\
**Post date:** [April 26, 2024, 6:00am UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/1 "2024-04-26T06:00:16Z")

</div>

There are some customers facing packet drop problems when using Windows computers to visualize the data from an OS lidar.

This problem might not happen for a 32 or 64-beam OS lidar because of the lower data volume per second. But for a 128-beam lidar, the high data rate, especially in dual return or 2048, 4096 lidar mode, can cause packet drop issues on a Windows computer without proper operating system configuration.

Under such condition, the packet drop problem is caused by Windows and not the lidar. Ouster lidars are engineered to drop zero packets across all operating modes and conditions, so long as they are used with a properly configured client network and computer.

**Example**  **Test Setup**  
Below is a picture to show that the points data from an OS lidar was broadcast to two computers with the same model (ThinkPad T490) but different Operating Systems (Windows 10 and Ubuntu 20.04).

 ![Broadcast lidar-data_Rviz&simpleViz](https://canada1.discourse-cdn.com/flex004/uploads/ouster/original/1X/924fc6e591eaa2c87e05351c24c56511bb0c59f6.jpeg)

The video can be found from the following link:  
[https://drive.google.com/drive/folders/154qFc3y2Fi3SLdwYYxQn6gFP83c72Bca?usp=sharing](https://drive.google.com/drive/folders/154qFc3y2Fi3SLdwYYxQn6gFP83c72Bca?usp=sharing)

If the packets are dropped by the lidar, the same loss of data in the point cloud should be observed on the two computers. In this case, only on the Windows 10 computer packet drop issue happened while on the Ubuntu computer points displayed smoothly without a packet drop.

This data broadcasting test can prove that lidar worked well and packet drop problem was not caused by the OS lidar.

**Solving Packet Drops on Windows 10**

This packet drop problem that happened to the Windows 10 computer can be solved by increasing the receive buffer. Here are the steps:

1. Go to Network Connections  
 ![1714110260349](https://canada1.discourse-cdn.com/flex004/uploads/ouster/original/1X/ad0888ef10172b3331b7530c05df9dfef3d49c26.png)
2. Right click the connection interface and choose Properties  
 ![1714110341303](https://canada1.discourse-cdn.com/flex004/uploads/ouster/original/1X/0e0df341d2e59c1e3ea4ab38ef39a02273ebde4b.png)
3. Click the Configure button  
 ![1714110495361](https://canada1.discourse-cdn.com/flex004/uploads/ouster/original/1X/98afb4aa6cbb080a46babb47b6e1f62bf4379d3f.png)
4. Click the Advanced tab  
 ![1714110538131](https://canada1.discourse-cdn.com/flex004/uploads/ouster/original/1X/8cf65ac6730d2344f4b8139377c9d6789f1c28b6.png)
5. Select the Receive buffers Property and increase the value to 1024 or 2048.  
 ![1714110634729](https://canada1.discourse-cdn.com/flex004/uploads/ouster/original/1X/af31d0ed974a35b30efb3f25f3364f59bba05a15.png)
6. Click OK to restart the network interface.

Then connect the lidar to the Windows 10 computer and visualise the points with OusterStudio or ouster-sdk visualisation tool.

Here in my test, I connected two 128-beam lidar sensors to the same Windows 10 computer, no packet drop problem arose again.

 ![Broadcast two lidar data to two PCs_ouster-cli and ros1](https://canada1.discourse-cdn.com/flex004/uploads/ouster/original/1X/295449dce715ce23bd5339e278f265911cf97914.jpeg)

The video can be found from the following link:  
[https://drive.google.com/drive/folders/154qFc3y2Fi3SLdwYYxQn6gFP83c72Bca?usp=sharing](https://drive.google.com/drive/folders/154qFc3y2Fi3SLdwYYxQn6gFP83c72Bca?usp=sharing)

---

<div class="post-metadata">

**Author:** ![Samahu](https://yyz2.discourse-cdn.com/flex004/user_avatar/community.ouster.com/samahu/32/39_2.png) [@Samahu](https://community.ouster.com/u/Samahu)\
**Post date:** [April 26, 2024, 2:46pm UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/2 "2024-04-26T14:46:47Z")

</div>

I could add that this also applies to other operation systems, not only Windows.

---

<div class="post-metadata">

**Author:** ![AndyN](https://avatars.discourse-cdn.com/v4/letter/a/8baadc/32.png) [@AndyN](https://community.ouster.com/u/AndyN)\
**Post date:** [April 28, 2024, 7:24pm UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/3 "2024-04-28T19:24:59Z")

</div>

If you’re seeing packet drops on a Linux device then there are a number of things you can try:

Firstly, you can query the receive buffer size by entering the following on the command line and looking at the Current hardware settings for RX:

```
	ethtool -g <network_interface>

```

Then try increasing the buffer size as much as possible (2048 for example) by entering the following command line:

```
	sudo ethtool -G <network_interface> rx 2048

```

Next set the MTU (Maximum Transmission Unit) to be as large as possible by entering the following command

```
	sudo ifconfig <network_interface> mtu 9000

```

In addition you can try changing the packet queue size using the following commands

```
	sudo sysctl -w net.core.rmem_max=16777216
	sudo sysctl -w net.core.rmem_default=16777216

```

This usually cures packet drops on Linux

---

<div class="post-metadata">

**Author:** ![kbear](https://yyz2.discourse-cdn.com/flex004/user_avatar/community.ouster.com/kbear/32/62_2.png) [@kbear](https://community.ouster.com/u/kbear)\
**Post date:** [June 17, 2024, 6:51pm UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/4 "2024-06-17T18:51:35Z")

</div>

Here is another set of Linux settings to try as well.

- Show UDP stats:
  - `cat /proc/net/udp`

- View current default UDP buffer:
  - `sudo sysctl net.core.rmem_default`

- Set max UDP buffer to 25MB:
  - `sudo sysctl -w net.core.rmem_max=26214400`

- Set default UDP buffer to 2MB:
  - `sudo sysctl -w net.core.rmem_default=2097151`

**Increase ipfrag buffer**

- Decrease UDP fragmentation buffer wait time (dump stale data faster)
  - `sudo sysctl -w net.ipv4.ipfrag_time=5`

- Increase UDP fragmentation buffer to 20 MB
  - `sudo sysctl -w net.ipv4.ipfrag_high_thresh=20000000`

- Increase UDP fragmentation buffer reset to 10 MB
  - `sudo sysctl -w net.ipv4.ipfrag_low_thresh=10000000`

If you need to return to default settings:

**Default**

- `sudo sysctl -w net.ipv4.ipfrag_low_thresh=196608`
- `sudo sysctl -w net.ipv4.ipfrag_high_thresh=262144`
- `sudo sysctl -w net.ipv4.ipfrag_time=30`

---

<div class="post-metadata">

**Author:** ![Jerome](https://avatars.discourse-cdn.com/v4/letter/j/a587f6/32.png) [@Jerome](https://community.ouster.com/u/Jerome)\
**Post date:** [January 21, 2025, 12:50pm UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/5 "2025-01-21T12:50:48Z")

</div>

Here is another way to increase Windows buffer that might help : [Add instructions for increasing Windows UDP receive buffer size · Issue #1 · lcm-proj/lcm-proj.github.io · GitHub](https://github.com/lcm-proj/lcm-proj.github.io/issues/1)

---

<div class="post-metadata">

**Author:** ![abdo](https://avatars.discourse-cdn.com/v4/letter/a/0ea827/32.png) [@abdo](https://community.ouster.com/u/abdo)\
**Post date:** [December 29, 2025, 6:33am UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/6 "2025-12-29T06:33:47Z")

</div>

Hi, I am using Windows 11, I have the same issue as mentioned here in this blog (packet drops) but my adapter in my laptop is out of range. [see the image attached].

Any other suggestions?

Thanks

 ![image](https://canada1.discourse-cdn.com/flex004/uploads/ouster/original/1X/272f2d6c05d46d1574a3aebdfd746df4256841ab.png)

---

<div class="post-metadata">

**Author:** ![Jerome](https://avatars.discourse-cdn.com/v4/letter/j/a587f6/32.png) [@Jerome](https://community.ouster.com/u/Jerome)\
**Post date:** [January 5, 2026, 3:31pm UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/7 "2026-01-05T15:31:38Z")

</div>

Hello Abdo,

It seems that your adapter prevents you to change the receive buffers setting to 2048. Is it a USB to Ethernet adapter ? If so can you try with another one ? or with another computer ?

Thank you.

---

<div class="post-metadata">

**Author:** ![mbries](https://avatars.discourse-cdn.com/v4/letter/m/ee7513/32.png) [@mbries](https://community.ouster.com/u/mbries)\
**Post date:** [January 13, 2026, 8:04pm UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/8 "2026-01-13T20:04:06Z")

</div>

Hi Abdo,

If your adapter does not go that high you can just set it as high as it allows (512). The specific setting value is not of particular importance. Doing that should avoid the issue in most cases, but if you still run into problems you will need to get a more capable ethernet adapter.

---

<div class="post-metadata">

**Author:** ![alex\_chua](https://avatars.discourse-cdn.com/v4/letter/a/dbc845/32.png) [@alex\_chua](https://community.ouster.com/u/alex_chua)\
**Post date:** [July 10, 2026, 8:58am UTC](https://community.ouster.com/t/increase-receive-buffer-to-eliminate-packet-drop-problem-on-some-windows-computers/84/9 "2026-07-10T08:58:09Z")

</div>

In Ubuntu, to permanently increase the UDP buffer

1. goto file `/etc/systemctl.d/99-sysctl.conf`

2. Add the following lines to the end of the files:

3. To apply changes without reboot, run:

To permanently increase the Rx buffer

1. Create a new systemd service file:  
`sudo nano /etc/systemd/system/set-ethtool.service`

2. Paste the following configuration into the file (replace `<sensor_network_interface>` with your actual interface name, e.g., `enp3s0` or `eth0`):

3. Enable and start the service so it runs automatically at every boot: